1.42.11.5 PWMx_ChannelPeriodGet Function
C
/* x = PWM instance number */ uint32_t PWMx_ChannelPeriodGet (PWM_CHANNEL_NUM channel); uint16_t PWMx_ChannelPeriodGet (PWM_CHANNEL_NUM channel);
Summary
Reads the period value of given PWM channel
Description
This function reads the period value of given PWM channel.
Precondition
PWMx_Initialize() function must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
channel | PWM channel |
Returns
The PWM channel's period value. Refer the generated header file for the exact return value type.
Example
uint16_t period;
PWM0_Initialize();
period = PWM0_ChannelPeriodGet(PWM_CHANNEL_0);
Remarks
Refer the generated header file for the exact function signature