1.42.11.4 PWMx_ChannelPeriodSet Function

C

/* x = PWM instance number */

void PWMx_ChannelPeriodSet (PWM_CHANNEL_NUM channel, uint32_t period);

void PWMx_ChannelPeriodSet (PWM_CHANNEL_NUM channel, uint16_t period);

Summary

Sets the period value of given PWM channel

Description

This function writes the period value in double buffer register. Update to the actual period register happens at the next period border.

Precondition

PWMx_Initialize() function must have been called first for the associated instance. And associated channel must be running.

Parameters

Param Description
channel PWM channel number
period period value corresponding to PWM frequency

Returns

None.

Example

PWM0_Initialize();
PWM0_ChannelsStart(PWM_CHANNEL_0_MASK);
PWM0_ChannelPeriodSet(PWM_CHANNEL_0, 0x500);

Remarks

Refer the generated header file for the exact function signature