1.11.3.11 CANx_TransmitEventFIFOElementGet Function

C

bool CANx_TransmitEventFIFOElementGet(uint32_t *id, uint32_t *sequence, uint32_t *timestamp) // x - Instance of the CAN peripheral

Summary

Get the Transmit Event FIFO Element for the transmitted message.

Description

This routine gets the Transmit Event FIFO Element for the transmitted message.

Precondition

CANx_Initialize must have been called for the associated CAN instance.

Parameters

Param Description
id Pointer to 11-bit / 29-bit identifier (ID) to be received.
sequence Pointer to Tx message sequence number to be received
timestamp Pointer to Tx message timestamp to be received, timestamp value is 0 if Timestamp is disabled in CFD${CAN_INSTANCE_NUM}TSCON

Returns

Request status. true - Request was successful.

false - Request has failed.

Example

uint32_t id, sequence, timestamp;
if (CAN1_TransmitEventFIFOElementGet(&id, &sequence, &timestamp))
{
    // Received id, sequence and timestamp on request success
}

Remarks

None.