1.5.23.30 TCCx_Compare24bitMatchSet Function

C

/* x = TCC instance number */
void TCCx_Compare24bitMatchSet( TCCx_CHANNEL_NUM channel, uint32_t compareValue );

Summary

Writes compare value of the given compare channel

Description

Set compare value of given channel

Precondition

TCCx_CompareInitialize() function must have been called first.

Parameters

Param Description
channel compare channel number
compareValue value to set for compare channel

Returns

None.

Example

uint32_t compareValue = 0x100;
TCC0_CompareInitialize();
TCC0_Compare24bitMatchSet(TCC0_CHANNEL0, compareValue);

Remarks

None