1.5.23.8 TCCx_Timer24bitCounterGet Function
C
/* x = TCC instance number */
uint32_t TCCx_Timer24bitCounterGet( void );
Summary
Reads the timer current count value.
Description
This function reads the timer count value.
Precondition
TCCx_TimerInitialize() function must have been called first.
Parameters
None.
Returns
Timer's current count value.
Example
uint32_t counter = 0;
TCC0_TimerInitialize();
TCC0_TimerStart();
counter = TCC0_Timer24bitCounterGet();
Remarks
The caller must know the number of significant bytes of timer. Period value is right-aligned.