1.14.2.6 CCPx_TimerFrequencyGet Function
C
/* x = CCP instance number */
uint32_t CCPx_TimerFrequencyGet( void );
Summary
Provides the given timer's counter-increment frequency.
Description
This function provides the frequency at which the given counter increments. It can be used to convert differences between counter values to real time or real-time intervals to timer period values.
Precondition
CCPx_TimerInitialize() function must have been called first.
Parameters
None.
Returns
frequency - The frequency (in Hz) at which the timer's counter increments.
Example
uint32_t frequency = 0;
CCP1_TimerInitialize();
frequency = CCP1_TimerFrequencyGet();
Remarks
None.