1.2.5.6 DMA_ChannelEnable Function
C
void DMA_ChannelEnable ( DMA_CHANNEL channel )
Summary
The function enables the specified DMA channel.
Description
The function enables the specified DMA channel. Once enabled, DMA will initiate a block transfer when the selected trigger is received
Precondition
DMA should have been initialized by calling DMA_Initialize.
Parameters
Param | Description |
---|---|
channel | The DMA channel that needs to be disabled |
Returns
None.
Example
// Enable the channel.
DMA_ChannelEnable (DMA_CHANNEL_0);
Remarks
None.