1.21.1.9 ADC_ResultGet Function
C
uint32_t ADC_ResultGet(ADC_RESULT_BUFFER bufferNumber) uint32_t ADC_ResultGet( ADC_CORE_NUM core, ADC_CHANNEL_NUM channel)
Summary
Returns the ADC conversion value.
Description
Returns ADC module conversion result based on the buffer index. Returns the ADC conversion value for the specified ADC core channel.
Precondition
ADC_Initialize() must have been called.
Parameters
Param | Description |
---|---|
bufferNumber | Selects the buffer to be read. |
core | ADC core n |
channel | ADC channel k |
Returns
uint32_t - ADC result value
Example
uint32_t my_res;
my_res = ADC_ResultGet(ADC_RESULT_BUFFER_0);
uint32_t adc_result; if (ADC_ChannelResultIsReady(ADC_CORE_NUM1, ADC_CH0)) { // ADC conversion is complete. Read the conversion result. adc_result = ADC_ResultGet(ADC_CORE_NUM1, ADC_CH0); }
Remarks
None.