1.25.23.7 TCx_CHy_TimerFrequencyGet Function
C
/* x = TC instance number, y= channel number */ uint32_t TCx_CHy_TimerFrequencyGet ( void );
Summary
Provides the given timer's counter-increment frequency.
Description
This function provides the frequency at which the given counter increments. It can be used to convert differences between counter values to real time or real-time intervals to timer period values.
Precondition
TCx_CHy_TimerInitialize() function must have been called first for the given channel.
Parameters
None
Returns
The frequency (in Hz) at which the timer's counter increments.
Example
uint32_t frequency; TC0_CH1_TimerInitialize(); frequency = TC0_CH1_TimerFrequencyGet();
Remarks
None