3.42.5 Hardened External Memory Controller (HEMC)

The HEMC System Memory interface provides a simple interface to manage the externally connected SDRAM, PROM and SRAM device.

Using The Library

The HEMC controller is initialized as configured in the MCC as part of System Initialization.

If interrupts are used, the callback function should be set for expected interrupts types:

    /* Register Fixable errors Callback */
    HEMC_FixCallbackRegister(HEMC_FixCallback_Function, (uintptr_t)NULL);
    /* Register UnFixable errors Callback */
    HEMC_NoFixCallbackRegister(HEMC_NoFixCallback_Function, (uintptr_t)NULL);

When an ECC error is detected and an interrupt occurs, the fail address must be read before the status in order to avoid multiple interrupts:

    /* Read the fault address before clearing the interrupt*/
    uint32_t* fault_pointer = (uint32_t*)HEMC_HeccGetFailAddress();

    /* Only for Fixable error handler : Read corrected data on the Fly */
    uint32_t fault_data = *fault_pointer;

    /* Read HEMC HECC Status */
    HEMC_HECC_STATUS value = HEMC_HeccGetStatus();

The faulty address may then be fixed by the application if applicable.

Error injection test mode

ECC Check bit read

The ECC check bit value can be get when the read test mode is activated. Once this mode is activated, the check bit value for each read of data on HSMC or HSDRAMC memories is stored in corresponding registers. It is possible to get the last check bit value using the \function HEMC_TestModeGetCbValue.

    /* Enable HEMC HECC Test mode Read in HSDRAMC memory */
    HEMC_TestModeReadEnable(HEMC_HEMC_CH_HSDRAMC);
    __DSB();
    __ISB();

    /* Read data in external memory */
    data = buffer;
    __DSB();
    __ISB();

    /* Get the Check Bit for last data read in HSDRAMC memory */
    tcb = HEMC_TestModeGetCbValue(HEMC_HEMC_CH_HSDRAMC);
    __DSB();
    __ISB();

    /* Disable HEMC HECC Test mode Read in HSDRAMC memory */
    HEMC_TestModeReadDisable(HEMC_HEMC_CH_HSDRAMC);

Note: It is recommended to use memory barriers on Cortex-M core-based products where instructions can be executed out of programmed order, or to ensure that all memory transfers or instructions are completed before any new instruction is executed. In our application, we must ensure that register modification and memory transfers are completed before executing the next step.

ECC Check bit write

The ECC check bit value can be override when the write test mode is activated. Once this mode is activated, the check bit value for each write of data on HSMC or HSDRAMC memories is override by the given value instead of being calculated automatically. The check bit value used should be set using the function HEMC_TestModeSetCbValue.

    /* Enable HEMC HECC Test mode Write in HSDRAMC memory */
    HEMC_TestModeWriteEnable(HEMC_HEMC_CH_HSDRAMC);
    __DSB();
    __ISB();

    /* Set the Check Bit for override when data will be write in external HSDRAMC memory */
    HEMC_TestModeSetCbValue(HEMC_HEMC_CH_HSDRAMC, tcb);
    __DSB();
    __ISB();

    /* Write data in external memory */
    buffer = data;
    __DSB();
    __ISB();

    /* Disable HEMC HECC Test mode Write in HSDRAMC memory */
    HEMC_TestModeWriteDisable(HEMC_HEMC_CH_HSDRAMC);

Note: It is recommended to use memory barriers on Cortex-M core-based products where instructions can be executed out of programmed order, or to ensure that all memory transfers or instructions are completed before any new instruction is executed. In our application, we must ensure that register modification and memory transfers are completed before executing the next step.

Library Interface

HEMC peripheral library provides the following interfaces:

Functions

NameDescription
HEMC_InitializeInitializes and Enables the HSDRAM and HSMC Controller
HEMC_HeccGetStatusGet the HECC status of the HEMC peripheral
HEMC_DisableECCDisable the ECC for the given chip select.
HEMC_EnableECCEnable the ECC for the given chip select.
HEMC_HeccGetFailAddressGet the last fail address were ECC error occurs in a HEMC memory
HEMC_HeccResetCountersReset Fix and NoFix error counters of the HEMC peripheral
HEMC_FixCallbackRegisterSets the pointer to the function (and it's context) to be called when the given HEMC's ECC Fixable Error interrupt events occur
HEMC_NoFixCallbackRegisterSets the pointer to the function (and it's context) to be called when the given HEMC's ECC Not Fixable Error interrupt events occur
HEMC_TestModeReadEnableEnable the HEMC peripheral HECC test mode Read
HEMC_TestModeReadDisableDisable the HEMC peripheral HECC test mode Read
HEMC_TestModeWriteEnableEnable the HEMC peripheral HECC test mode Write
HEMC_TestModeWriteDisableDisable the HEMC peripheral HECC test mode Write
HEMC_TestModeGetCbValueGet the HEMC peripheral HECC test mode check bit values
HEMC_TestModeSetCbValueSet the HEMC peripheral HECC test mode check bit values
HEMC_Write8Writes 8 bit data at given address.
HEMC_Write16Writes 16 bit data at given address.
HEMC_Write32Writes 32 bit data at given address.
HEMC_Read8Read 8 bit data at the given address.
HEMC_Read16Read 16 bit data at the given address.
HEMC_Read32Read 32 bit data at the given address.

Data types and constants

NameTypeDescription
HEMC_HEMC_CHANNELEnumIdentifies the HEMC HECC channel
HEMC_HECC_STATUSEnumIdentifies the HEMC HECC current status
HEMC_CALLBACKTypedefHEMC Callback Function Pointer