3.39.17 Two-wire Interface - TWI
The TWI PLIB can be configured in TWI master mode.
TWI master mode The TWI peripheral library supports the following transfers:
Master Write: The master writes a block of data to the slave Master Read: The master reads a block of data from the slave Master Write/Read: The master writes and then reads back a block of data from slave.
The block of data is transferred in a non-blocking manner using a peripheral interrupt. Application can either use a callback or IsBusy API to check for completion of data transfer.
// Following code demonstrates TWI write operation using polling method #define APP_SLAVE_ADDR 0x0057 #define NUM_BYTES 10 uint8_t myWriteData [NUM_BYTES] = {'1', '0', ' ', 'B', 'Y', 'T', 'E', 'S', '!', '!',}; int main(void) { /* Initialize all modules */ SYS_Initialize ( NULL ); /* Write data to the TWI Slave */ TWI1_Write(APP_SLAVE_ADDR, &myWriteData[0], NUM_BYTES); /* Poll and wait for the transfer to complete */ while(TWI1_IsBusy()); /* Check if any error occurred */ if(TWI1_ErrorGet() == TWI_ERROR_NONE) { //Transfer is completed successfully } else { //Error occurred during transfer. } ... }
// Following code demonstrates TWI write operation using callback method #define APP_SLAVE_ADDR 0x0057 #define NUM_BYTES 10 uint8_t myWriteData [NUM_BYTES] = {'1', '0', ' ', 'B', 'Y', 'T', 'E', 'S', '!', '!',}; void TWI1_Callback(uintptr_t context) { if(TWI1_ErrorGet() == TWI_ERROR_NONE) { //Transfer is completed successfully } else { //Error occurred during transfer. } } int main(void) { /* Initialize all modules */ SYS_Initialize ( NULL ); /* Register Callback function */ TWI1_CallbackRegister(TWI1_Callback, (uintptr_t)NULL); /* Submit Write Request */ TWI1_Write(APP_SLAVE_ADDR, &myWriteData[0], NUM_BYTES); ... }
Library Interface
TWI Mode
Functions
| Name | Description |
|---|---|
| TWIx_Initialize | Initializes given instance of the TWI peripheral |
| TWIx_Read | Reads data from the TWI slave |
| TWIx_Write | Writes data to the TWI slave |
| TWIx_WriteRead | Write and Read data from TWI Slave |
| TWIx_IsBusy | Returns the TWI Peripheral busy status |
| TWIx_ErrorGet | Returns the TWI error that occurred on the bus |
| TWIx_TransferSetup | Dynamic setup of TWI Peripheral |
| TWIx_CallbackRegister | Sets the pointer to the function (and it's context) to be called when the given TWI's transfer events occur |
| TWIx_BusScan Function | Scans and reports the target devices found on the bus |
Data types and constants
| Name | Type | Description |
|---|---|---|
| TWI_ERROR | Enum | Defines the possible errors that the I2C peripheral can generate in I2C master mode |
| TWI_TRANSFER_SETUP | Struct | I2C transfer setup data structure |
| TWI_CALLBACK | Typedef | Defines the data type and function signature for the TWI peripheral callback function in TWI master mode |