2.128.10 TWI_ERROR Enum
C
/* TWI master mode */
typedef enum
{
/* No Error */
TWI_ERROR_NONE,
/* Slave returned Nack */
TWI_ERROR_NACK,
} TWI_ERROR;
Summary
Defines the possible errors that the TWI peripheral can generate in master mode.
Description
This enum defines the possible errors the TWI peripheral can generate when it is configured in master mode. An error of this type is returned by the TWIx_ErrorGet() function.
Remarks
None.