2.128.5 TWIx_IsBusy Function
C
/* x = TWI instance number */
/* TWI master mode */
bool TWIx_IsBusy(void)
Summary
Returns the TWI Peripheral busy status.
Description
This function returns true if TWI module is busy with a transfer. The application can use this function to check if TWI module is busy before calling any of the data transfer functions. The library does not allow a data transfer operation if another transfer operation is already in progress.
Precondition
TWIx_Initialize must have been called for the associated TWI instance.
Parameters
None.
Returns
true - Busy
false - Not busy
Example
// wait for the current transfer to complete while(TWI1_IsBusy());
Remarks
None