3.12.15 Quad Serial Peripheral Interface (QSPI)
The Quad SPI Interface (QSPI) is a synchronous serial data link that provides communication with external devices in Master mode. It is similar to SPI protocol except that it has additional data lines.
The QSPI can be used in normal SPI mode or in Serial Memory mode to connect to external Flash memories. The normal SPI has four communication lines: Chip Select, Clock, MOSI, and MISO. For QSPI, additional data lines are available. The command/data/address are sent through single, dual, quad or octa IO based on the mode selected.
As data is sent over multiple lines, it helps in increasing bandwidth compared to a standard SPI transfer. With the support of the Quad SPI protocol, the QSPI allows the system to use high-performance serial Flash memories which are small and inexpensive, in place of larger and more expensive parallel Flash memories.
The QSPI allows the system to execute code directly from a serial Flash memory (XIP) without code shadowing to RAM. The serial Flash memory mapping is seen in the system as other memories such as SRAM, and FLASH memory.
Using The Library
The QSPI Peripheral Library operates in Serial Memory Mode or SPI Mode to interface with the QSPI based Serial Flash Memories operating in Single-bit SPI, Dual SPI, Quad SPI and Octa SPI.
The QSPI Peripheral library provides non-Blocking API's, which can be used to perform the following functionalities on the QSPI Slave device.
-
Send a command
-
qspi_command_xfer_t data type needs to filled to send a command to the slave device
-
-
Register read/write
-
qspi_register_xfer_t data type needs to be filled to read data from a register or to write data to a register.
-
-
Memory read/write
-
qspi_memory_xfer_t data type needs to be filled to read data from flash memory or to write data to the FLASH memory.
-
Here is an example code to read data from MX66 QSPI flash memory using QSPI peripheral
#define MX66_CMD_OCTA_8READ 0xEC13 static qspi_memory_xfer_t qspi_memory_xfer; static uint32_t buffer[256]; uint32_t address = 0x0 memset((void *)&qspi_memory_xfer, 0, sizeof(qspi_memory_xfer_t)); qspi_memory_xfer.instruction = MX66_CMD_OCTA_8READ; qspi_memory_xfer.width = OCT_CMD; qspi_memory_xfer.dummy_cycles = 20; qspi_memory_xfer.addr_len = ADDRL_32_BIT; qspi_memory_xfer.protocol_type = OCTAFLASH; if (QSPI0_MemoryRead(&qspi_memory_xfer, buffer, sizeof(buffer), address) == false) { // Handle Error }
Library Interface
Quad Serial Peripheral Interface peripheral library provides the following interfaces:
Functions
QSPI Mode:
| Name | Description |
|---|---|
| QSPIx_Initialize | Initializes given instance of the QSPI peripheral |
| QSPIx_CommandWrite | Writes command to QSPI slave device |
| QSPIx_RegisterRead | Reads particular register of QSPI slave device |
| QSPIx_RegisterWrite | Writes to particular register of QSPI slave device |
| QSPIx_MemoryRead | Reads from the specified address of the serial flash device |
| QSPIx_MemoryWrite | Writes to the specified address of the serial flash device |
SPI Mode:
| Name | Description |
|---|---|
| QSPIx_Initialize | Initializes given instance of the QSPI peripheral |
| QSPIx_TransferSetup | Setup QSPI operational parameters as desired by the client. |
| QSPIx_WriteRead | Write and Read data on QSPI peripheral. |
| QSPIx_Write | Write data on QSPI peripheral. |
| QSPIx_Read | Read data on QSPI peripheral. |
| QSPIx_IsBusy | Returns transfer status of QSPI peripheral. |
| QSPIx_CallbackRegister | Allows application to register callback with PLIB. |
Data types and constants
| Name | Type | Description |
|---|---|---|
| QSPI_ADDRESS_LENGTH | Enum | Defines the data type to specify address length |
| QSPI_LANE_WIDTH | Enum | Defines the data type to specify lane width |
| QSPI_OPTION_LENGTH | Enum | Defines the data type to specify option length |
| QSPI_PROTOCOL_TYPE | Enum | Defines the QSPI Protocol type - STD_SPI, TWIN_QUAD, OCTAFLASH and HYPERFLASH |
| QSPI_CLOCK_PHASE | Enum | Identifies QSPI Clock Phase Options |
| QSPI_CLOCK_POLARITY | Enum | Identifies QSPI Clock Polarity Options |
| QSPI_DATA_BITS | Enum | Identifies SPI bits per transfer |
| QSPI_TRANSFER_SETUP | Struct | Identifies the setup parameters which can be changed dynamically |
| qspi_command_xfer_t | Struct | Defines the data type for the QSPI commands transfer |
| qspi_register_xfer_t | Struct | Defines the data type for the QSPI register data transfer |
| qspi_memory_xfer_t | Struct | Defines the data type for the QSPI memory transfer |
| QSPI_CALLBACK | Typedef | Pointer to a Callback function. This is used in SPI mode only |