25.4.9 EEPROM Objects
The __eeprom qualifier can be used to indicate that variables should be
positioned in EEPROM.
Use the native keywords discussed in the Differences section to look up information on the semantics of this qualifier.
Some devices may not implement EEPROM. Use of this qualifier for such devices generates a
warning. Stack-based (auto and parameter) variables cannot use the
__eeprom specifier.
Example
The following shows a variable qualified using __eeprom.
__eeprom int serialNos[4];
Differences
The 8-bit compilers have used the qualifier, eeprom, to indicate this
meaning for some devices.
The 16-bit compilers have used the space attribute to allocate variables
to the memory space used for EEPROM.
Migration to the CCI
For 8-bit compilers, change any occurrence of the eeprom
qualifier to __eeprom, for example, from:
eeprom char title[20];
to:
__eeprom char title[20];
For 16-bit compilers, change any occurrence of the eedata space
attribute to __eeprom, for example, from:
int mainSw __attribute__ ((space(eedata)));
to:
int __eeprom mainSw;
Caveats
MPLAB XC8 does not implement the __eeprom qualifiers for any PIC18
devices; this qualifier works as expected for other 8-bit devices.