25.4.8 Alignment of Objects
The __align(alignment)
specifier can be used to
indicate that variables must be aligned on a memory address that is a multiple of the
alignment specified. The alignment term must be a power of 2. Positive values request
that the object’s start address be aligned.
Use the native keywords discussed in the Differences section to look up information on the semantics of this specifier.
Example
__align()
to ensure they end on an address that is a multiple of 8, and start on an address that
is a multiple of 2,
respectively.__align(-8) int spacer;
__align(2) char coeffs[6];
Differences
The MPLAB XC16, XC-DSC and XC32 compilers have used the aligned
attribute with variables. This has also been true when targeting AVR MCUs with MPLAB XC8
An alignment feature has never been available for PIC devices when using the MPLAB XC8
compiler.
Migration to the CCI
When building for AVR MCUs with the MPLAB XC8 compiler or when using any other compiler,
change any occurrence of the aligned
attribute to the
__align
specifier, for example, from:
char __attribute__((aligned(4)))mode;
to:
__align(4) char mode;
Caveats
This feature is not needed nor implemented when targeting PIC devices using MPLAB XC8.
When targeting PIC32C/SAM devices with MPLAB XC32 only positive alignment values are supported.