29.1.14 __builtin_section_end Built-in Function
Remember: This built-in function
gets run-time information about section addresses and sizes.
Description
Return the end address of the quoted section name + 1.
Prototype
unsigned long __builtin_section_end(quoted-section-name);
Argument
quoted-section-name The name of the section.
Return Value
The end address of the section + 1.
Assembler Operator/ Machine Instruction
.endof.
Error Messages
An “undefined reference” error message will be displayed if the quoted section name does not exist in the link.