30.2.4.3 I2C Host Mode Reception
Host mode reception (see Figure 30-31) is enabled by setting the Receive Enable (RCEN) bit.
Important: The MSSP module must be in an Idle state before the RCEN bit is set or the RCEN bit will be disregarded.
The Baud Rate Generator begins counting and on each rollover, the
state of the SCL pin changes (high-to-low/low-to-high) and data is shifted into the SSPxSR.
After the falling edge of the eighth clock all the following events occur:
The MSSP is now in Idle state awaiting the next command. When the buffer is read by the CPU, the BF flag bit is automatically cleared. The Host can then send an Acknowledge sequence at the end of reception by setting the Acknowledge Sequence Enable (ACKEN) bit.