17.3 External Analog Reference Connections

The following schematic checklist is only necessary if the application is using one or more of the external analog references. If the internal references are used instead, the following circuits in Figure 17-3 and Figure 17-4 are not necessary.

Figure 17-3. External Analog Reference Schematic With Two References
Figure 17-4. External Analog Reference Schematic With One Reference
Table 17-2. External Analog Reference Connections
Signal NameRecommended Pin ConnectionDescription
VREFx1.0V to (VDDANA – 0.6V) for ADC 
Decoupling/filtering capacitors
100 nF(1)(2) and 4.7µF(1)External reference VREFx for the analog port
GND—Ground
Note:
  1. These values are only given as a typical example.
  2. It is recommended that the decoupling capacitor be placed close to the device for each supply pin pair in the signal group.