14.9 Reset Values
The reset values of the AT86RF212B registers in state P_ON(1, 2, 3) are shown in the table below.
Note: All reset values in the table below are only valid after a power on reset. After a
reset procedure (/RST = L), the reset values of selected registers (for example
registers 0x01, 0x10, 0x11, 0x30) can differ from the reset values listed in the
table.
| Address | Reset Value |
|---|---|
| 0x00 | 0x00 |
| 0x01 | 0x00 |
| 0x02 | 0x00 |
| 0x03 | 0x19 |
| 0x04 | 0x20 |
| 0x05 | 0x60 |
| 0x06 | 0x00 |
| 0x07 | 0xFF |
| 0x08 | 0x25 |
| 0x09 | 0x77 |
| 0x0A | 0x17 |
| 0x0B | 0xA7 |
| 0x0C | 0x24 |
| 0x0D | 0x01 |
| 0x0E | 0x00 |
| 0x0F | 0x00 |
| Address | Reset Value |
| 0x10 | 0x00 |
| 0x11 | 0x02 |
| 0x12 | 0xF0 |
| 0x13 | 0x00 |
| 0x14 | 0x00 |
| 0x15 | 0x00 |
| 0x16 | 0x31 |
| 0x17 | 0x00 |
| 0x18 | 0x58 |
| 0x19 | 0x00 |
| 0x1A | 0x48 |
| 0x1B | 0x40 |
| 0x1C | 0x07 |
| 0x1D | 0x03 |
| 0x1E | 0x1F |
| 0x1F | 0x00 |
| Address | Reset Value |
| 0x20 | 0xFF |
| 0x21 | 0xFF |
| 0x22 | 0xFF |
| 0x23 | 0xFF |
| 0x24 | 0x00 |
| 0x25 | 0x00 |
| 0x26 | 0x00 |
| 0x27 | 0x00 |
| 0x28 | 0x00 |
| 0x29 | 0x00 |
| 0x2A | 0x00 |
| 0x2B | 0x00 |
| 0x2C | 0x38 |
| 0x2D | 0xEA |
| 0x2E | 0x42 |
| 0x2F | 0x53 |
| Address | Reset Value |
| 0x30 | 0x00 |
| 0x31 | 0x00 |
| 0x32 | 0x00 |
| 0x33 | 0x00 |
| 0x34 | 0x3F |
| 0x35 | 0x00 |
| 0x36 | 0x00 |
| 0x37 | 0x00 |
| 0x38 | 0x00 |
| 0x39 | 0x40 |
| 0x3A | 0x00 |
| 0x3B | 0x00 |
| 0x3C | 0x00 |
| 0x3D | 0x00 |
| 0x3E | 0x00 |
| 0x3F | 0x00 |
Note:
- While the reset value of register 0x10 is 0x00, any practical access to the register is only possible when DVREG is active. So this register is always read out as 0x04.
- While the reset value of register 0x11 is 0x02, any practical access to the register is only possible when BATMON is activated. So this register is always read out as 0x22 in P_ON state.
- While the reset value of register 0x30 is 0x00, any practical access to the
register is only possible when the radio transceiver is accessible. So the
register is usually read out as:
- 0x11 after a reset in P_ON state
- 0x07 after a reset in any other state