28.5.2.2 Initialization
Before enabling event routing within the system, the Event Users Multiplexer and Event
Channels must be selected in the Event System (EVSYS), and the two peripherals that
generate and use the event have to be configured. The recommended sequence is as
follows:
- In the peripheral generating the event, enable output of event by writing a '1' to the respective Event Output Enable bit ("EO") in the peripheral's Event Control register (for example, TCC.EVCTRL.MCEO1, AC.EVCTRL.WINEO0, or RTC.EVCTRL.OVFEO).
- Configure the EVSYS:
- Configure the Event User multiplexer by writing the respective EVSYS.USERm register, refer to User Multiplexer Setup.
- Configure the Event Channel by writing the respective EVSYS.CHANNELn register, refer to Event System Channel.
- Configure the action to be executed
by the event user peripheral by writing to the Event Action bits (EVACT) in the
respective Event control register (for example, TC.EVCTRL.EVACT, PDEC.EVCTRL.EVACT).
Note: This step is not required for all peripherals.
- In the event user peripheral, enable event input by writing a '1' to the respective Event Input Enable bit ("EI") in the peripheral's Event Control register (for example, AC.EVCTRL.IVEI0, ADC.EVCTRL.STARTEI).