58.4.2 Backup Mode Entry and Wake-up

The following figure shows the recommended power-down sequence to place the SAM9X60 in Backup mode. The SHDN signal, output of Shutdown Controller (SHDWC), signals the shutdown request to the external power supply. This output is supplied by VDDBU that is present in Backup mode. In a similar way to the power-down sequence, the NRST signal must be asserted prior to turning the SAM9X60 power supplies off.

Figure 58-4. Recommended Power Sequence at Backup Mode Entry
Table 58-10. Backup Mode Entry Timing Requirements
SymbolParameterConditions(1)MinMaxUnit
tSHDNSHDN Delay at Backup mode entryDelay from SHDN low to NRST low0–ms
tRSTPDNRST Delay at power-downDelay from NRST low to the first supply out of its operating range0–ms

The following figure shows the recommended power-up sequence to wake up SAM9X60 from Backup mode. Upon a wake-up event (WKUP pin, RTC alarm, etc.), the Shutdown Controller automatically toggles its SHDN output back to VDDBU to request the external power supply to restart. This power-up sequence is the same as the one shown in figure Recommended Power Sequence at Power-up. In particular, the supply group’s definition is the same.

Figure 58-5. Recommended Power Sequence at Wake-up from Backup Mode
Table 58-11. Wake-up from Backup Mode Timing Requirements
SymbolParameterConditionsMinMaxUnit
t0VDDIN33 delayDelay from SHDN high to VDDIN33 turn-on0–ms
t1VDDIN33 to periphery group delayDelay from VDDIN33 established to the first periphery group supply established0–ms
t2Periphery group to VDDCORE delayDelay from the last periphery group established supply to VDDCORE supply turn-on0–ms
t3Reset delay at power-upFrom VDDCORE established to NRST high8–ms
Note:
  1. The term "established" refers to a power supply established to 90% of its final value.