3.4 Immunity
Immunity describes the robustness of an application. It is the type and level of injected
            disturbances that can be handled by the application prior to the malfunction occurrence.
            Examples are:
        - In-band disturber (Signal to Noise Ratio (SNR))
 - Blocking
 
Note: A conducted influence can propagate and turn to a radiated
                emission that influences other applications.
Even if an application passes the
            certification, it does not mean that there are no disturbances. It only says that the
            unwanted radiated signals are below the threshold. For the application, this might
            result in the situation that it will disturb themselves. A simple example would be an
            RF-based control of an engine. If the engine is off, the system has an excellent
            performance, but once the engine is started, the RF performance becomes poor. The reason
            for such an effect is the worsened SNR caused by the engine. That means the application
            disturbs its own RF communication. Such use cases must be validated by the application
            developer team as the performance validation is not part of the certification.