3.7.2 Steps to Configure Low-Power

  1. Configure the Button n as a Low-Power button by writing 1 to the Low-Power Sensor (LP) bit in the Sensor Control (SENCTRL) register.

    Note: If one or more of the buttons are not set to be low-power buttons, the device will not go into Low-Power mode.
  2. Enable Low-Power mode by writing 1 to the Low-Power (LP) bit in the Device Control (DEVCTRL) register.
    Note: Calibration and Suspension of Button n should not be enabled (Refer to the Sensor Control (SENCTRL) register).

Refer to the Configuration Summary for more details.