11.1.6 I/O Characteristics
The device features two types of Input/Output (I/O) circuits:
- GPIO
- DDRIO
Unless otherwise specified:
- The following specifications apply to the GPIO type.
- VDD refers to the voltage of the associated power rail of the I/O line, as defined in the Pin Description table. For example, for PA2, VDD refers to the voltage applied on VDDIOP0.
- The GPIO type drive and slewrate controls are set in the PIO_DRIVE and PIO_SLEWR registers, respectively.