Table 16-6. Commands Available through the SAM-BA Monitor
Command
Action
Argument(s)
Example
N
Set Normal Mode
No argument
N#
T
Set Terminal Mode
No argument
T#
O
Write a byte
Address, Value#
O200001,CA#
o
Read a byte
Address,#
o200001,#
H
Write a half word
Address, Value#
H200002,CAFE#
h
Read a half word
Address,#
h200002,#
W
Write a word
Address, Value#
W200000,CAFEDECA#
w
Read a word
Address,#
w200000,#
S
Send a file
Address,#
S200000,#
R
Receive a file
Address, NbOfBytes#
R200000,1234#
G
Go
Address#
G200200#
V
Display version
No argument
V#
Mode commands:
Normal mode configures SAM-BA Monitor to send / receive data in binary
format,
Terminal mode configures SAM-BA Monitor to send / receive data in ASCII
format.
Write commands: Writes a byte (O), a halfword (H) or a word (W) to the target
Address: Address in hexadecimal
Value: Byte, halfword or word to write in hexadecimal
Output: ‘>’
Read commands: Reads a byte (o), a halfword (h) or a word (w) from the target
Address: Address in hexadecimal
Output: The byte, halfword or word read in hexadecimal followed by ‘>’
Send a file (S): Sends a file to a specified address
Address: Address in hexadecimal
Output: ‘>’
Note: There is a timeout on this command which is reached when
the prompt ‘>’ appears before the end of the command
execution.
Receive a file (R): Receives data into a file from a specified address
Address: Address in hexadecimal
NbOfBytes: Number of bytes in hexadecimal to receive
Output: ‘>’
Go (G): Jumps to a specified address and executes the code
Address: Address to jump to in hexadecimal
Output: ‘>’ once returned from the program execution. If the executed
program does not handle the link register at its entry and does not return,
the prompt is not displayed.
Get Version (V): Returns the Boot Program version
Output: version, date and time of ROM code followed by ‘>’
DS60001476L
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.