3.2.1 Host PC with On-Board MCP2200 USB-to-UART Converter

The simplest method to use the RNWF11 UART to Cloud Add On Board is to connect it to a PC host that supports USB CDC virtual COM (serial) ports using the on-board MCP2200 USB-to-UART Converter. The user can send simple ASCII commands to the RNWF11PC Module by using a terminal emulator application. In this situation, the PC acts as the host device. In addition to UART, status and other control GPIOs from the RNWF11PC Module are also connected to MCP2200 GPIO pins.
Note: The MCP2200 is configured in Reset condition until the USB supply is plugged in.
Table 3-3. RNWF11PC Connection to MCP2200 USB-to-UART Converter

Pin on MCP2200

Pin on RNWF11PC Module

Description

TXUART1 RXDRNWF11PC Module UART RXD
RXUART1 TXDRNWF11PC Module UART TXD
RTSPA11, UART1 CTSRNWF11PC Module UART CTS
CTSPA13, UART1 RTSRNWF11PC Module UART RTS
GP0——
GP1——
GP2NMCLRRNWF11PC Module Reset pin
GP3PA10, WAKE_INPUT/INT0Wake input
GP4PB12, IRQInterrupt
GP5——
GP6——
GP7——
Note:
  1. The MCP2200 automatically enters a Reset state when the USB cable is not connected. If using the mikroBUS, there is no need to manually disable the MCP2200. The users can easily switch the power selection header (J5) based on whether the board is used in a standalone scenario or as a mikroBUS host.

  2. The power selection header (J5) provides a solution for exceptional cases where the USB cable needs to be plugged in for power when using mikroBUS, a scenario not typical for the board’s default design. When utilizing the mikroBUS connector, the power is intended to be supplied from the mikroBUS 3V3.