37.2.7.2.1 Enable/Disable Target Events Command (ENEC/DISEC)

The Controller uses the Direct and Broadcast ENEC/DISEC set of CCCs to control whether Target-initiated traffic is allowed on the bus or not. This governs whether a Target on the bus can perform any of following three requests:

  • In-Band Interrupt (IBI) Request
  • Controller Role Request(1)
  • Hot-Join Request

Figure 37-22 shows the frame format for Direct Write ENEC/DISEC CCC, whereas Figure 37-23 shows the frame format for Broadcast Write ENEC/DISEC CCC. Table 37-12 and Table 37-13 show the command byte for ENEC and DISEC respectively. The information received from the Controller is stored in the I3CxEC Event Commands register.

Figure 37-22. Direct Write ENEC/DISEC Frame Format
Figure 37-23. Broadcast Write ENEC/DISEC Frame Format
Table 37-12. Enable Target Events Command Byte Format
Bit 7Bit 6Bit 5Bit 4Bit 3Bit 2Bit 1Bit 0
ReservedENHJReservedENCRENINT
Table 37-13. Disable Target Events Command Byte Format
Bit 7Bit 6Bit 5Bit 4Bit 3Bit 2Bit 1Bit 0
ReservedDISHJReservedDISCRDISINT
The ENINT/DISINT (IBIEN bit in the I3CxEC register) allows the Controller to control when a Target can perform an IBI request. When enabled (ENINT), the Controller instructs the Target that performing IBI requests is permitted on the bus. When disabled (DISINT), the Controller instructs the Target that performing IBI requests is not permitted on the bus and that any such requests may not be honored.
The ENHJ/DISHJ (HJEN bit in the I3CxEC register) allows the Controller to control when a Target can perform a Hot-Join request. When enabled (ENHJ), the Controller instructs the Target that performing Hot-Join requests is permitted on the bus. When disabled (DISHJ), the Controller instructs the Target that performing Hot-Join requests is not permitted on the bus and that any such requests may not be honored. The Controller can choose to broadcast this CCC to instruct devices to refrain from making Dynamic Address Assignment requests until later authorized by the Controller, in case the Controller is unable to service the Hot-Joining devices.
Important: This I3C Target module does not support Secondary Controller features. Controller role request (ENCR/DISCR) in the command byte will be ignored and the CREN bit in the I3CxEC register will always read ‘0’.