8.4.4 Transfer the OTAU bin file to the iPhone
This document for the OTA update procedure refers to iPhone only. For Android mobile, follow the same procedure.
iPhone
Copy the OTAU file to MBD by email.
- Send the OTAU bin file to the personal email account via email.
- Open the attached OTAU file.
- Tap the share icon (see the
following figure).
Figure 8-20. Microchip Bluetooth Data Interface
- Tap the MBD icon (see the
following figure). After launching the MBD application, the OTAU file is copied
to the MBD inbox folder.
Figure 8-21. Save Firmware to MBD