5.7.1 Serial DFU Procedure
In this method, the RNBD350 device is configured into DFU mode to support the serial firmware update.
The DFU commands are, then, sequentially passed to the device starting with a DFU update request
command (DFUU). The device, then, responds back with a maximum fragment
image size as its approval to accept the firmware update request. The maximum fragmented
size is the range at which the RNBD350 device
can receive the data. The DFU firmware update, then, starts with a DFU Update Start
(DFUS) command and a continuous sequence of DFU image distribution
commands. The DFU image Distribution (DFUD) command appends the
firmware data in fragmented size not greater than the maximum size proposed by the RNBD350 device. All commands must be in ASCII
format, except the payload parameter in the DFUD (image distribution)
command, which must be in raw hex format to increase the transmission performance. The
DFU image distribution command is passed until the complete firmware file data is passed
to the RNBD350 device. After image transmission
completion, the DFU Update Complete (DFUC) command is issued to
indicate the completion and request RNBD350 to
perform validation. The newly-passed firmware image is, then, validated by the RNBD350 device and responds back the with a
status message. Upon receiving a %VALIDATION_SUCCESS% response from the
RNBD350, the DFUE command
is employed to reboot the device, signifying a successful update. For more details on
the demo procedure, refer to RNBD350 Device Firmware Update Procedure.
To exit the DFU mode on the RNBD350, the complete command sequence must be followed successfully. Otherwise, the device will remain in the DFU mode. The users cannot forcibly switch from the DFU mode to the Command mode by simply plugging in or unplugging the USB cable.
The following conditions happen in RNBD350:
- In CMD mode:
- MCU may send command to change baud rate
- MCU sends
DFUcommand to enter DFU mode
- Enter DFU mode:
- Disconnect all links, disable ADV activity and SCAN activity
- Disable Sleep mode
- Disable all interrupts
- Erase metadata block of application firmware
- Reboot to enter secondary bootloader
- In DFU mode:
- DFU abort, validation error, timeout occurred and error occurred will be at DFU mode
- Reset to jump to the new image when the validation is successful