4.5 UART Mode Switch (PA9)
- When the host MCU pulls the UART mode switch pin from low to high (rising edge), the RNBD350 module switches to Data mode.
- When the host MCU pulls the UART mode switch pin from high to low (falling edge), the RNBD350 module switches to Command mode.
- When the host MCU uses the RN command to switch the mode, the host MCU keeps the UART mode switch pin to the original setting.
Note:
- By default, the UART mode switch
functionality is not assigned to the PA9 pin. The user can enable this feature
using the
SR,<hex16>command, for example,SR,0002. For more details, refer to Set Application Options. - If using PA9 for GPIO, do not enable pull-up or pull-down: use external resistors.