The
I2CxCNT register can be automatically loaded. Auto-loading of
the I2CxCNT register is enabled when the Auto-Load I
2C Count Register Enable
(
ACNT) bit is set (ACNT =
1).
In Host Transmit mode, the first byte following either the 7-bit or 10-bit client address
is transferred from I2CxTXB into both I2CxCNT and the transmit shift register.
In Host Reception mode, the first byte received from the client is loaded into both
I2CxCNT and
I2CxRXB. The value of the Acknowledge Data (
ACKDT)
bit is used as the host’s acknowledgment response to prevent a false NACK from being
generated before the I2CxCNT register is updated with the new count value.
In Client Reception mode, the first byte received after receiving a matching 7-bit or
10-bit address is loaded into both I2CxCNT and I2CxRXB, and the value of the ACKDT bit
is used as the client’s acknowledgment response.
In Client Transmit mode, the first byte loaded into I2CxTXB following the reception of a
matching 7-bit or 10-bit address is transferred into both I2CxCNT and the transmit shift
register.
Important: It is not necessary to
preload the I2CxCNT register when using the auto-load feature. If no value is loaded by
the 9th falling SCL edge following an address transmission or reception, the Byte Count
Interrupt Flag (
CNTIF) will be set by module hardware and must be cleared by software to
prevent an interrupt event before I2CxCNT is updated. Alternatively, I2CxCNT can be
preloaded with a non-zero value to prevent the CNTIF from being set. In this case, the
preloaded value will be overwritten once the new count value has been loaded into
I2CxCNT.