5.10 Public Key Generation
Store the public key in the U-Boot Control DTB and then merge it with the U-Boot binary as follows:
- Copy u-boot.dtb into the
buildroot-mchp directory and rename it to
u-boot-pki.dt:
$ cp output/build/uboot-linux4microchip-2026.04/u-boot.dtb ./u-boot-pki.dtb - Copy u-boot-nodtb.bin to the
buildroot-mchp
directory:
$ cp output/build/uboot-linux4microchip-2026.04/u-boot-nodtb.bin . - Run the mkimage tool located
in the U-Boot build directory to create a FIT image and extract the public key. Make
sure that the signing key and certificate are located in the same directory. In this
example, the directory is named keys. The keys directory should
contain the following files: samkey.crt and samkey.key.
samkey.crt is the certificate, and samkey.key is the private key
used to sign the FIT
file.
$ output/build/uboot-linux4microchip-2026.04/tools/mkimage -v -f sam9x75_secure.its -k keys -r -K u-boot-pki.dtb sam9x75_secure.itb - To concatenate
u-boot-nodtb.bin and the control DTB with the public
key:
$ cat u-boot-nodtb.bin u-boot-pki.dtb > u-boot.bin