5.4 OpenSSL Configuration File
Before creating the certificates that will be used to sign the code images, the default OpenSSL configuration file should be modified. The modifications include changing the default values for the “distinguished name” found in certificates and creating “key usage” values for the code signing certificate.
The procedure is as follows:
- Create a directory to store the
configuration file, keys and
certificates:
$ mkdir keys $ cd keys - Copy the default OpenSSL
configuration:
$ cp /etc/ssl/openssl.cnf . - Edit the configuration file
(openssl.cnf) to fill in the req_distinguished_name section with values
that represent your
organization:
[ req_distinguished_name ] countryName = Country Name (2 letter code) countryName_default= US countryName_min= 2 countryName_max= 2 stateOrProvinceName = State or Province Name (full name) stateOrProvinceName_default = Arizona localityName = Locality Name (eg, city) localityName_default = Chandler 0.organizationName= Organization Name (eg, company) 0.organizationName_default = Microchip Technology - Create a section named code_sign
with the following fields:
[ code_sign ] basicConstraints=CA:FALSE keyUsage = digitalSignature extendedKeyUsage = codeSigning subjectKeyIdentifier=hash authorityKeyIdentifier=keyid,issuer