5.9 FIT Template
FIT files are created by the mkimage tool using a DTS-syntax input file. The mkimage tool relies on the Device-Tree-Compiler as part of the process for creating the signed FIT file. The U-Boot version of DTC has the /incbin/ reserved word, which allows an entire binary image to be included as the value of a property in the final DTB. This is how the Linux® kernel and Linux DTB are placed into the FIT file.
In the buildroot-mchp directory, create a file named sam9x75_secure.its with
the following content:
/dts-v1/;
/ {
description = "My FIT Image";
#address-cells = <1>;
images {
kernel-1 {
description = "Linux4SAM Linux kernel";
data = /incbin/("./output/images/zImage");
type = "kernel";
arch = "arm";
os = "linux";
compression = "none";
load = <0x22000000>;
entry = <0x22000000>;
hash-1 {
algo = "sha256";
};
};
fdt-1 {
description = " SAM9X75-Curiosity Flattened Device Tree blob";
data = /incbin/("./output/images/at91-sam9x75_curiosity.dtb");
type = "flat_dt";
arch = "arm";
compression = "none";
hash-1 {
algo = "sha256";
};
};
};
configurations {
default = "conf-1";
conf-1 {
description = " Linux kernel and FDT blob for SAM9X75-Curiosity board";
kernel = "kernel-1";
fdt = "fdt-1";
signature-1 {
algo = "sha256,rsa4096";
key-name-hint = "samkey";
sign-images = "fdt", "kernel";
};
};
};
};