14 Support Documentation

This section has documentation that is generic and used as supporting document with the application example documentation.

14.1 User Action

This document explains the code edits needed after a user generates a code using MPLAB Code Configurator.

Developers are required to call API - app_idle_task() in vApplicationIdleHook(). This is required to enable periodic Persistent Data Storage, RF calibration. Persistant Data Storage provides means for storing data in non-volatile memory(Flash). User application and stack parameters like peer connection etc are saved. IDLE task is set to execute at the lowest priority in FreeRtos.

  1. Users are prompted to call app_idle_task() and app_idle_updateRtcCnt(RTC_Timer32CounterGet()) when they compile/build the project with a compile error.

    Action required to be taken

  2. users are required to open freertos_hooks.c file and add #include "definitions.h"

  3. Users are required to open freertos_hooks.c file and add API app_idle_task()

  4. Users are required to comment out #error in app_user_edits.c file

  5. Initiate build and user will be able to build successfully

Note: User action is only required for the first time code gets generated.

Additional User Action when Low Power is Enabled

Developers are required to call app_idle_updateRtcCnt(RTC_Timer32CounterGet()) in vApplicationTickHook(). This API call is used to compensate for FreeRTOSTimer when in sleep mode.
  1. Users are required to open freertos_hooks.c file and add API app_idle_updateRtcCnt(RTC_Timer32CounterGet())

14.2 MPLAB Code Configurator (MCC) Code Generation

  1. Generate a code.
  2. Select Generate.

Merge Strategy

For more details on Merge Strategy and its understanding, refer to MPLAB® Code Configurator (MCC) Classic in Reference Documentation.

Note: Select “Close” the merge window to maintain the modifications made for the application code development.