10 Low Power Design

This section provides detailed instructions on enabling low power modes, specifically Sleep/Standby and Deep Sleep/Backup modes, in the design.

10.1 Low Power Design on PIC32-BZ6 Devices

The PIC32-BZ6 examples and protocol stacks include support for Sleep and Deep Sleep Low Power modes within the Harmony framework for the PIC32-BZ6 devices. In this context, Sleep and Deep Sleep modes are equivalent to Standby and Backup modes, respectively. For consistency, this online reference guide refers to Sleep mode as Standby and Deep Sleep mode as Backup.

The following are the differences between Sleep and Deep Sleep Low Power mode:

  1. Sleep Low Power Mode:
    1. Application layer calls Bluetooth® Low Energy stack to enable advertising. The Bluetooth Low Energy stack continues sending and receiving advertising Tx and Rx periodically until the application layer disables it.
    2. The system continues to operate between Active mode and Sleep mode periodically based on the advertising Tx and Rx.
    3. The application layer can have peripherals running in Sleep/Standby Low Power mode.
  2. Deep Sleep Low Power Mode:
    1. Application layer calls Bluetooth Low Energy stack to enable Deep Sleep Advertisement. The Bluetooth Low Energy stack backs up advertisement parameters and data into backup SRAM and perform one time advertising event.
    2. After entering Deep Sleep Low Power mode, the system wakes up from reset, resulting in loss of all parameters. Backup SRAM (retained in Deep Sleep Low Power mode) stores the advertisement parameters for recovery after reset.
    3. Application layer puts the system into Deep Sleep Low Power mode and controls the wake-up time based on RTC timer (which runs in Deep Sleep Low Power mode).
    4. Once the system wakes up from Deep Sleep Low Power mode, the application layer triggers advertisement again by recovering the advertisement and data parameters stored in backup SRAM.

Low-power design of a system involves optimizing power both in hardware and software. To name a few:

  • System Design:
    • MLDO vs Buck mode (DC/DC), operating in the Buck mode yields to power consumption savings.
    • Board design must allow measurement of the current consumed by the PIC32-BZ6 device alone, as multiple components can be present in the system.
    • Ensure to verify device errata, with special attention to issues that affect device power consumption.
    • Lower system clock speed from 64 MHz to 48 MHz; some applications can operate with a lower system clock speed of 48 MHz.
  • Hardware Design:
    • Configuring the transmitter power at 0 dBm with Buck mode on at 64 MHz, the PIC32-BZ6 device draws 22.72 mA.
      • At +12 dBm transmitter (Buck mode at 64 MHz) current consumption is 42.82 mA.
      • At +4 dBm transmitter (Buck mode at 64 MHz) current consumption is 24.98 mA.
      • At power up, all GPIO’s are inputs. Ensure to configure the unused GPIOs as input and pull down configuration.
  • For more details on software design, refer to the Low Power BLE Application Design from Related Links.

10.2 Low Power BLE Application Design

When developing a wireless Bluetooth® application, the advertisement and connection intervals managed by the BLE stack play a key role in determining when the device enters and exits sleep modes. The BLE stack supports two types of Low-power or Sleep modes:

  • Sleep
  • Deep Sleep

Sleep and Deep Sleep modes are equivalent to Standby and Backup modes, and these terms may be used interchangeably throughout this online reference guide.

The following table lists the various functionality/modules of the device that are available in the Low-power modes supported by the BLE stack.

Table 10-1. Device Functionality in BLE Low Power Modes
FunctionSleepDeep Sleep
Legacy ADVAvailableAvailable
Extended ADV (coded PHY)AvailableNot supported
BLE connectionAvailableThe device can begin advertising while in the Deep Sleep Low-power mode and, after establishing a BLE connection, transition to the Sleep low power mode.
PeripheralsAvailable(1)Limited wake-up sources are available
Device wakes up from reset after exiting the Sleep modeNoYes
System RAMAvailableNot retained
Backup RAMNot used by application or BLE stackAvailable and used by application and BLE stack
Timer used to manage sleep and wake-up timesWireless subsystem manages time intervals based on ADV/connection intervals setup by API calls to BLE stack libraryRTC
ADV intervals recommendedNo minimum/maximum ADV intervalMinimum ADV interval = 500 ms for power consumption savings
Note:
  1. For more details, refer to the Highly Integrated Wireless MCU with CAN FD, Ethernet, USB, Motor Control, Graphics, Touch and Enhanced Security Data Sheet (DS00005998) in the Reference Documentation from Related Links.

10.2.1 Sleep/Standby Low Power Mode

Application Sleep Duration Control

The BLE stack enables the system to enter Low Power mode when there is no ongoing data transmission or reception, or during the BLE advertisement or connection intervals. The system sleep is managed automatically by the stack and cannot be directly controlled through a parameter or API call.

Device Operation in Sleep Low Power Mode

While the system is in the Sleep mode, it disables the system PLL clock and the stops system tick. The user must adjust the FreeRTOS timer to account for the duration spent in Low Power mode. The RTC timer can continue running during low power modes and corrects the FreeRTOS timer offset.

Factors such as BLE activity intervals, external interrupts (for example, GPIO), or peripheral interrupts determine the total time the system spends in Sleep mode. Peripherals permitted to operate in Standby or Sleep Low Power mode can continue functioning during the Sleep mode. In Deep Sleep or Backup mode, only specific peripherals, such as the RTC and INT0, can remain active.

Enabling Sleep/Standby Low Power Mode

Table 10-2 10-4. Reference Application Examples
Application Example DescriptionReference
BLE Sleep Mode Legacy AdvertisementsImplements Sleep Low Power mode with periodic BLE legacy advertisements.See BLE Legacy Advertisements from Related Links.
BLE Extended AdvertisementsImplements Sleep Low Power with periodic BLE extended (coded PHY) advertisements.See BLE Extended Advertisements from Related Links.
BLE SensorImplements sleep low power mode in a BLE connection oriented application and data exchange using Microchip transparent UART service. This application also has peripherals that are enabled to run in Standby/Sleep Low Power mode.See BLE Sensor from Related Links.
BLE Custom ServiceImplements Sleep Low Power in a BLE connection oriented application and data exchange using custom service. This application does not have peripherals continuing to run in Standby/Sleep Low Power modeSee BLE Custom Service from Related Links.

Generating Sleep Mode Code with MPLAB Code Configurator

  1. The user must enable the system Sleep Mode in BLE stack H3 component configuration. After enabling this, the system requests to enable dependent components like RTC (timer source during sleep).
    Figure 10-1. Enable Sleep Mode
  2. Upon enabling Sleep mode, the system automatically sets the FreeRTOS related settings.
    1. In the “RTOS Configuration” drop-down menu, perfrom the following steps:
      1. Set the “Tick Mode” to Tickless_Idle. This allows the system to suppress periodic tick interrupts when idle, reducing power consumption.
      2. Set the “Expected idle time before sleep” to 5 (ms).
      Figure 10-2. FreeRTOS Settings
    2. Enabling Tick Hook.
      1. Find the option labeled “Tick Hook.”
      2. Check the Use Tick Hook. This allows the user to add custom code that executes during each tick interrupt.
      Figure 10-3. Tick Hook
    3. RTC peripheral library will be added and configured.
      Note: RTC counter must not be reset (RTC_Timer32CounterSet()) arbitrarily when the system is running.
  3. The user must manually set the RTC clock source, the following are the four options:
    1. FRC (±1% offset)
    2. LPRC (with larger offset, < ±5%)
    3. POSC – Candidate of the clock source (better clock accuracy)
    4. SOSC – Candidate of the clock source (better clock accuracy)
    Note: Select POSC/SOSC as the RTC clock source, as other clock sources can impact BLE connection stability.
    Figure 10-4. Clock Configuration
  4. Manually setting RTC clock source – POSC.
    1. Choose “POSC” in “Clock Configuration”.
    2. The user must configure as illustrated in the following figure.
    Figure 10-5. Manually Setting RTC Clock Source – POSC
  5. Manually Setting RTC clock source – SOSC, by turning on SOSC and then choose SOSC as illustrated in the following figure.
    Figure 10-6. Manually Setting RTC Clock Source – SOSC
    Note: The users can only select one clock source POSC or SOSC, steps mention how to choose either.
  6. All unused pins in the application needs to be set to Input mode and the pull-down must be enabled for these pins.
    1. The user can configure this through pin configuration in Harmony3 Configurator. For more details, see the following figure.
    Figure 10-7. Pin Settings
  7. For more details on code generation, refer to the MPLAB Code Configurator (MCC) Code Generation from Related Links.

Sleep-Related Code Implementation Locations

Table 10-3. Sleep-Related Code Implementation Locations
ImplementationLocation
BT Sleep ModeBLE stack library
System Sleep Modedevice_sleep.c
Execute BT/System Sleepapp_idle_task.c
RTC Based Tickless Idle Modeapp_idle_task.c

User Code for Sleep/Standby Low Power Mode Entry

FreeRTOS provides Tickless IDLE mode for power saving, allowing the user can to stop periodic tick interrupts during idle periods (periods when no application tasks can execute). To account for the lost time during the IDLE mode, the user can use the RTC timer to make a correcting adjustment to the RTOS tick count value when it restarts (after waking up from sleep). For more information on Low Power Tickless mode, refer to the Low Power Support in Reference Documentation from Related Links. The system automatically executes the Tickless Idle mode when the Idle task is the only task able to run because all the application tasks are either in Blocked or Suspended state. To prevent the system from entering Sleep/Standby Low mode and waking up immediately, it automatically sets the minimum sleep time (IDLE time) to 5 ms.
Note: Maximum sleep time is equal to the maximum period of the RTC 32-bit counter, 134217.8 second (around 37 hours).
  1. In order for the system to enter Sleep mode, the system needs to request Bluetooth® wireless subsystem to sleep. This is accomplished by calling the BT_SYS_EnterSleepMode() API for BLE.
    Figure 10-8. BT_SYS_EnterSleepMode() API
  2. The API to call to ensure subsystem is sleeping (inactive) or ready for system to enter Sleep mode is the BT_SYS_AllowSystemSleep API.
    Figure 10-9. BT_SYS_AllowSystemSleep API
  3. If the expected sleep time is greater than 5 ms, the system is allowed to enter Sleep mode by checking for two conditions:
    1. Bluetooth subsystem is inactive.
    2. eTaskConfirmSleepModeStatus() returns eNoTasksWaitingTimeout. For more information, refer to the eTaskConfirmSleepModeStatus in Reference Documentation from Related Links.
    Note: The user can also add their own condition to be checked before system goes to sleep, for example, do not enter system sleep if data transmission over UART is active.
    Pseudo code in RTC based Tickless Idle Mode:
    
    ```
    if ((BT_SYS_AllowSystemSleep()) && ( eTaskConfirmSleepModeStatus() != eAbortSleep ) && (user_condition))
    {
            //Enter System Sleep Mode
            DEVICE_EnterSleepMode ();        //RTC Based Tickless Idle Mode       
    }
    ```
  4. When both the conditions as mentioned in point 3 are met, enter RTC based Tickless Idle mode (stops the system tick, uses the RTC timer to set the sleep time, disables interrupts).
    1. The system enters Sleep mode after setting the RTC based Tickless Idle mode by calling Device_EnterSleepMode()API and then the system executes the Wait for Interrupt (WFI) instruction.
      Figure 10-10. RTC Based Tickless Idle Mode Entry Sequence

Exiting Sleep Mode

When the system is in Sleep or Standby Low Power mode, it can be awakened by one of the following events:
  • RTC timeout
  • BLE event
  • GPIO interrupt
To exit Sleep mode, perform the following steps:
  1. Calling DEVICE_ExitSleepMode() API to begin the wake-up process.
  2. After exiting the Sleep mode, interrupts must be re-enabled to allow execution of the interrupt service routines.
  3. Interrupts are initially disabled because the system tick needs to be compensated (as required by Tickless IDLE mode in FreeRTOS).
    Figure 10-11. Exiting Sleep Mode Flow Chart
Figure 10-12. Hardware and Firmware State during System Wake Up and Sleep Mode

10.2.2 Deep Sleep/Backup Low Power Mode

Application Control of Sleep Duration

The user application controls how long the device remains in Deep Sleep Low Power mode. When the user sets the advertisement interval and enables Deep Sleep mode in the BLE_Stack component within the MCC, the system automaticalluy generates all necessary APIs for entering and exiting Deep Sleep. The user application must enable deep sleep advertising and manage the sleep and wake-up durations according to the chosen advertisement interval.

Unlike Sleep mode, which relies on a timer within the wireless subsystem to manage sleep and wake-up periods, the Deep Sleep mode does not have access to this timer. Instead, the RTC timer available during Deep Sleep wakes the device through its interrupt, configured according to the Deep Sleep advertisement interval. The user can transition the device into Deep Sleep Low Power mode after receiving the BLE_GAP_EVT_ADV_COMPL event from the BLE stack.

Device Operation in Deep Sleep Low Power Mode

When the application layer initiates the BLE stack to enable deep sleep advertising, the BLE stack backs up advertising parameters and application data into backup RAM and performs a one-time advertisement event.

The application layer then puts the system in Deep Sleep mode and controls deep sleep wake-up time using the RTC timer. The user is responsible for putting the system into Deep Sleep mode and controlling the wake-up using the RTC.

Based on the RTC Timer interval, the device wakes up from Deep Sleep Low Power mode. Exiting Deep Sleep mode is similar to Power-On Reset (POR). Backup RAM saves the adv parameters through a reset; upon wake-up, the BLE stack is able to continue advertising based on the data retained in backup RAM.

Device Start-Up and Initialization Timing

The start-up and initialization code for the device differs and optimizes to enable fast completion of initialization after a reset caused by waking up from Deep Sleep Low Power mode. The MCC generates the DEVICE_DeepSleepIntervalCal API to calibrate the sleep duration based on the advertising interval chosen. The device’s start-up and initialization procedures optimize to make the device enter Deep Sleep Low Power mode as soon as possible. The device spends approximately 10 ms during start-up and firmware initialization. The average start-up time for the device is 1.5 ms. The firmware initialization time for various applications can change based on the user’s choice of peripherals and clocks to initialize.

Maintaining I/O State after Reset in Deep Sleep Mode

The device needs to back up all GPIO register settings before entering Deep Sleep mode and recover these settings when the device wakes up from deep sleep, before clearing the Deep Sleep (DSCON) register. The following API, clears this register.
DEVICE_ClearDeepSleepReg()

MPLAB Code Configurator Usage for Deep Sleep Mode

  1. In MPLAB® X IDE, open MCC and create a new Harmony project.
  2. Add required components to the Project Graph.
    Note: The application being developed determines whether some components are optional.
    Figure 10-13. Deep Sleep Mode Project Graph
  3. Select the BLE Stack in the Project Graph tab.
    1. Configure the following settings for “BLE stack” component. The slower the advertising interval, the less current consumption. User can select their desired interval.
      Figure 10-14. BLE Stack Configuration Options Settings
  4. Select “RTC” component in the Project Graph tab.
    1. Configure the following settings for “RTC” component.
      Figure 10-15. RTC Component Configuration Options Settings
  5. Go to MPLAB® Code Configurator>Harmony>Clock Configuration.
    1. Go to Clock Diagram in MCC.
    2. Set LPCLK source to POSC. From the drop-down list, select POSC.
    Figure 10-16. Clock Configuration
    Figure 10-17. Manually Setting RTC Clock Source – POSC
    Figure 10-18. POSC Configuration bits Generated after Code Generation
  6. Go to MPLAB® Code Configurator>Harmony>Clock Configuration.
    1. Go to Clock Diagram in MCC.
    2. Set LPCLK source to SOSC. From the drop-down list, select SOSC.
      Figure 10-19. Manually Setting RTC Clock Source – SOSC
      Figure 10-20. SOSC Configuration bits Generated after Code Generation
  7. Clock Switching mechanism , if LPCLK source is set as POSC clock source using clock configuration, the FW switch to LPRC as LPCLK source as POSC clock source is unavailable in Deep Sleep Low Power Mode.

Enabling Deep Sleep/Backup Low Power Mode

Table 10-2 10-4. Reference Application Examples
Application Example DescriptionReference
BLE Deep Sleep AdvertisingOn reset, the device starts in Deep Sleep mode. Pressing the SW1 button on the curiosity board starts the system’s Deep Sleep Advertisements. Once a central device connects, the device switches to Sleep Low Power mode.See BLE Deep Sleep Advertising from Related Links.

Recommendations for Deep Sleep Advertisement Mode

Ensure to use Deep Sleep Advertisement mode when the advertisement interval is >= 500 ms.

Supported BLE Advertisement Types in Deep Sleep Mode

When using Deep Sleep mode, the system supports BLE legacy advertisement types ADV_IND, ADV_SCAN_IND, ADV_DIRECT_IND_LOW, and ADV_NONCONN_IND.

Retaining Application Data in Backup RAM

The user must define the variable as persistent. Persistent variables are variables that the runtime start-up code must not clear, such as during a reset. The user must initialize a persistent variable as follows. The data read/write into backup RAM must be single word (4 bytes).

uint32_t __attribute__((persistent)) backup1;

The user firmware must not assign initial values for persistent variables.

Bootloader Firmware Authentication in Deep Sleep Mode

If firmware authentication is enabled in the bootloader, it checks for Firmware Authentication upon all types of resets like POR, BOR, and more. The device skips firmware authentication only when it wakes up from Deep Sleep Low Power mode.

Recommended RTC Clock Sources for Deep Sleep Mode

The recommendation is to use SOSC or LPRC as the clock sources when using the Deep Sleep mode.