8 Write Sequence
To program the AT25080B/AT25160B, two separate instructions must be
executed. First, the device must be write-enabled using the Write Enable
(
WREN) instruction. Then, one of the two write sequences described
in this section may be executed. Note: If
the device is not write-enabled (
WREN), it will ignore the
WRITE instruction and return to the Standby state when
CS is brought high. A new CS
assertion is required to reinitiate communication.The address of the memory location(s) to be programmed must be outside the protected
address field location selected by the block write protection level. During an internal
write cycle, all commands except the
RDSR instruction are ignored.
Refer to Table 8-1 for the AT25080B/AT25160B address bits.| Address | AT25080B | AT25160B |
|---|---|---|
| AN | A9–A0 | A10–A0 |
| Don’t Care Bits | A15–A10 | A15–A11 |