5 TX Mode Does Not Work as Expected
- Have you checked the proper
connection of the external components?
- Are the antenna or the analyzer connected?
A bad connection can lead to a drop in the output power or a total loss of the signal.
- Are you using the device in a 3V or
5V application?
- Have you connected the 3V to VS_PA?
- Have you set the correct VS_PA setting in the EEPROM configuration?
Depending on the product, it might be necessary to define the power supply level in the EEPROM configuration.
- Have you measured the current
consumption, and what is the value?
An incorrect current consumption can be an indication of an incorrect mode.
- Have you triggered VCO tuning during
the start-up of a mode?
VCO tuning is required to ensure that the PLL is able to lock under all conditions.
- Do you use the Buffered mode?
- Have you set the right buffer threshold values in EEPROM?
- Have you loaded the SFIFO and DFIFO with data?
- Have you followed the SFIFO guidance?
In Buffered mode, it is required to load the transmission data into the internal buffer. Also, the start conditions must be set correctly.
- Was there a receive event prior to
the transmission?
- Have you read all the data from SFIFO upfront?
Any data from an earlier reception might still be present in the buffer if not accessed earlier. In such a case, the transmission might be corrupted. Therefore, it is recommend that the buffer be cleared prior to using it for the transmit function.
- Do you use the Transparent mode?
- Have you added the data signal to the TMDI pin?
Depending on the modulation, no RF signal is present as long as no signal is present at the TMDI pin.