2.3.2 ESMC RX Subsystem
(Ask a Question)ESMC RX subsystem consists of the following modules:
- pdu_parser: It implements a FIFO management system to detect and store the ESMC PDU by checking the Destination Address (48'h0180_C200_0002).
- Header decoder
- Storing pdu
- pdu_checker: This module handles the following features:
- pdu_info_extraction: A finite state machine decodes and stores the data fields from the received PDU.
- ql_priority_selection_algo: Logic to compares the local QL value with the decoded QL value and selects the QL value which has higher priority (better clock quality).
- pdu_generation_request: When ql_enabled is "0", a DNU info pdu send request is sent to the pdu_generator, whereas when ql_enabled is "1", pdu_checker module sends a pdu generation request to pdu_generator based on the result of QL selection logic.
- Port availability information
The following figure shows the PDU checker finite state machine.
PDU checker finite state machine traverses through the following states when any of the send PDU requests are received:
The Enabling Jitter Cleaner mode has the following scenarios:
- After reset is de-asserted enable_japll signal is "1", when pdu_data_ready signal is "1", pdu_checker will deassert the JAPLL by setting enable_japll to "0".
- This sequence is performed only once when ql_enable is "1" to show the actual working of the jitter cleaner PLL.
- Enable_japll will remain "0", until there is any change in the input QL value.
- If the QL selection logic detects a change in the input QL value, enable_japll becomes "1" for the transmitter to lock to the new clock reference which has a better clock quality than the local reference clock.