4.7.11 _strncpy_packed Function
Copies at most len bytes of a string from one
__pack_upper_byte Flash buffer to another buffer in RAM.
Include
<libpic30.h>
Prototype
void* _strcpy_packed( void *dest, __pack_upper_byte void
*src, int len);
Arguments
dest | destination memory address |
src | address of data to be written |
len | length of program memory |
Return Value
The string pointed to by dest.
Remarks
None.
Default Behavior
Copy at most len bytes of the string pointed to by
src to the RAM buffer pointed to by dest. Unlike
the standard strncpy function, this function does not zero fill the
remaining space in the destination string.
File
memcpy_helper.s