4.7.7 _strcpy_packed Function
Copies a string from one __pack_upper_byte Flash buffer to
another buffer in RAM.
Include
<libpic30.h>
Prototype
void* _strcpy_packed( void *dest, __pack_upper_byte void
*src);
Arguments
dest | destination memory address |
src | address of data to be written |
Return Value
The string pointed to by dest.
Remarks
None.
Default Behavior
Copy the string pointed to by src to the RAM buffer pointed
to by dest. Unlike the standard strncpy function, this
function does not zero fill the remaining space in the destination string.
File
memcpy_helper.s