4.5 CLASSB_Init
Function
static CLASSB_INIT_STATUS CLASSB_Init(void);
Summary
This function is executed on every device reset. This shall be called right after the reset, before any other initialization is performed.
Description
This function performs the following:
a. It initializes the global variables used by the Class B library.
b. Checks the reset cause and decides next course of action.
c. If the reset is not caused by the Class B library, it tests the reserved SRAM area, clears all self-test results and performs a WDT test.
Precondition
None.
Parameters
None.
Returns
CLASSB_SST_DONE if all SSTs are successfully executed.
CLASSB_SST_NOT_DONE if SSTs are yet to be executed.
Example
CLASSB_INIT_STATUS init_status = CLASSB_Init();
Remarks
None.