1.7.1.4 Live Update Memory Layout for MIPS Based MCUs

  • Supported for the devices which have a Dual Bank Flash memory

  • Switcher code is placed at start of the Boot Flash memory (0xBFC00000) as upon reset the device runs from start of boot Flash memory

    Note: The switcher code provided does not have any programming capabilities. It just performs bank swap operations.
  • Device always executes the application firmware from PFM bank mapped to lower memory region (0x1D00_0000 Physical address)

    • Start address of Active Bank is mapped to lower region 0x9D000000

    • Start address of Inactive Bank is from mid of the PFM which can vary from device to device. Refer to the respective Data Sheets for details of Flash memory layout.

  • Row size number of bytes are reserved at end of each bank for storing serial number. This serial number will be used by the switcher code placed in BFM to map the appropriate PFM bank to lower memory region and run the application from there.

  • Volatile register SWAP bit is used to map either of bank to lower memory region by switcher

  • The bootloader live update code responsible to program the inactive bank is part of the application it self. Which means the programming operation can happen while the application is running.

    • Live Update Application = (Bootloader Code in Live Update mode + Application code)
  • The application code is responsible to send a request to bootloader live update code to perform a bank swap and reset to run the new firmware programmed in Inactive bank

  • Once this request is received the bootloader live update code performs below operation before initiating a reset to run new firmware

    • Inactive Serial number = Active serial number + 1
  • At reset switcher first maps Bank 1 to lower region and reads the serial numbers from both banks

  • If Bank 2 serial number is greater than Bank 1 serial number, it maps Bank 2 to lower region by setting the Swap bit and runs the new firmware. So, Bank 2 is Active bank.

  • The live update start address should always fall into lower mapped region (0x9D000000 to Mid of Flash). Size of the application in the linker script should also not exceed the Mid of Flash.