1.7.1 How the UDP Bootloader Library Works
The UDP Bootloader firmware communicates with the Unified Host application running on Host PC by using a predefined communication protocol.
The UDP Bootloader works in two different modes:
Basic Mode
-
This mode is supported for all the devices
-
Resides from:
-
The starting location of the Flash memory region for Cortex-M based MCUs
-
The starting location of the Boot Flash memory region or Program Flash memory region for MIPS based MCUs devices
-
-
The Bootloader performs Flash erase/program/verify operations with the application hex sent from host PC using the Unified Bootloader Host Application while in the Firmware Upgrade mode
-
Bootloader always performs Flash operation from the address received via hex record
-
The application can use the entire Flash memory region starting from the end of bootloader space
-
-
Jumps to the application once programming is completed
Live Update Mode
-
This mode is supported for the devices which have a Dual Bank Flash memory
-
Resides from
-
The starting location of the Flash memory region of both the banks on Cortex-M based MCUs along with application code
-
The starting location of the Program Flash memory region of both the banks for MIPS based MCUs devices along with application code
-
-
The Bootloader task performs Flash erase/program/verify operations with the application hex sent from host PC using the Unified Bootloader Host Application in the Inactive bank
-
Performs a bank swap and reset to run the application programmed in inactive bank on application task request