1.2.3.2 Bootloader Linker Configurations for Cortex-M Based MCUs
Linker configurations for the UART, I2C and CAN Bootloaders
-
Bootloader library uses a custom linker script which is generated through MCC
-
The values populated in the linker script are based on the Bootloader component MCC configurations
-
Bootloader is configured to run from RAM in this linker script to achieve simultaneous Flash memory write and reception of the next block of data.
Note: The below sections provides overview of changes done to bootloader linker scripts when compared to default linker script. The <bootloader_start> address and <bootloader_length> may vary based on the specific device used.
#define ROM_START <bootloader_start> /* Bootloader size is calculated with below criteria with optimization level -O2 * bootloader size = Minimum Flash Erase Size Or actual bootloader ELF size (Rounded of to nearest erase boundary) whichever is greater. */ #define ROM_SIZE <bootloader_length> /* Bootloader Trigger pattern needs to be stored in starting <trigger_len> Bytes * of Ram by the application if it wants to run bootloader at startup without any * external trigger. * Example: * ram[0] = 0x5048434D; * ram[1] = 0x5048434D; * .... * ram[n] = 0x5048434D; */ #define RAM_START (<ram_start> + <trigger_len>) #define RAM_SIZE (<ram_length> - trigger_len) MEMORY { rom (rx) : ORIGIN = ROM_START, LENGTH = ROM_SIZE ram (rwx) : ORIGIN = RAM_START, LENGTH = RAM_SIZE } SECTIONS { /* * Configure to place the vector table in Flash but to be run from RAM */ .vectors : { . = ALIGN(4); _sfixed = .; KEEP(*(.vectors .vectors.*)) } > ram AT > rom .text : { . = ALIGN(4); .... .... . = ALIGN(4); _efixed = .; /* End of text section */ } > rom .... .... . = ALIGN(4); _etext = .; /* Locate text/rodata in special data section to be copied to RAM in startup sequence. */ .data : { . = ALIGN(4); __data_start__ = .; _sdata = .; *(.dinit) *(.text) *(.text.*) *(.rodata) *(.rodata.*) . = ALIGN(4); __data_end__ = .; _edata = .; } > ram AT > rom .... }
Custom startup file for UART, I2C and CAN Bootloaders
-
To reduce the size of the binary these bootloaders make use of custom startup file which is generated by MCC
-
This startup file places only the Reset handler in vector table instead of populating all the device vectors there by reducing the size of final .vector section
-
This startup file also copies the entire bootloader code placed in .data section above from Flash to RAM as it is built to run from RAM
/* Declaration of Reset handler (may be custom) */ void __attribute__((noinline)) Reset_Handler(void); __attribute__ ((used, section(".vectors"))) void (* const vectors[])(void) = { &_ram_end_, Reset_Handler, }; ... ... /* Linker-defined symbols for data initialization. */ extern uint32_t _sdata, _edata, _etext; extern uint32_t _sbss, _ebss; void __attribute__((noinline, section(".romfunc.Reset_Handler"))) Reset_Handler(void) { uint32_t *pSrc, *pDst;; pSrc = (uint32_t *) &_etext; /* flash functions start after .text */ pDst = (uint32_t *) &_sdata; /* boundaries of .data area to init */ /* Copy code from flash to RAM using .data section */ while (pDst < &_edata) *pDst++ = *pSrc++; /* Init .bss */ pDst = &_sbss; while (pDst < &_ebss) *pDst++ = 0; .... .... }
MPLAB X Setting for UART, I2C and CAN Bootloaders
-
Below MPLAB X option is enabled by MCC for these bootloaders to remove the XC32 crt0 startup code
-
By disabling this crt0 startup code, further reduce the size as it removes the default initialization mechanism code by XC32