4.1.1.3 Estimation of Maximum Frequency Offset between Receiver and Transmitter

The required channel filter bandwidth depends on the frequency error between the receiver and transmitter and the occupied bandwidth of the modulation signal used. For ASK systems, a frequency transition during the power amplifier switching has to be additionally taken into account if the ATA8510/15 is used as the ASK transmitter. For more details, see the ASK considerations in the second part of this section.

System Design with Compensation of Initial XTAL and XTO Tolerances shows the main impact of the XTO on the worst case frequency error between the receiver and transmitter. The maximum frequency error between the receiver and transmitter has to be determined for the individual application, and the channel filter bandwidth has to be chosen with enough width to prevent the unintentional loss of sensitivity, in the case of worst case frequency errors. The channel bandwidths of the ATA8510/15 can be configured between 25 kHz and 360 kHz. The required register settings are described in Channel Filter Bandwidths.

The following table shows the measured frequency offset values with 1.5 dB sensitivity loss for FSK systems compared with values calculated using equation (51). If using NRZ encoding instead of Manchester encoding, equation (51) can be used, replacing data rate (DR) by symbol rate (SR). The calculated maximum frequency offset differs from measurement in cases of high occupied bandwidth compared to the channel filter bandwidth and in cases of high modulation indices. This behavior is a property of the RxDSP; therefore, it is highly reproducible and a measurement result can be used for system design without the need to consider part-to-part variations.
ΔfS1.5dBFSK⁢ =  BWIF2− DRFSK2⁢ + fDEV2......(51)
DR⁢=SR2......(52)
Table 4-1. Filter Settings for Each Supported IF Bandwidth

Channel Filter Bandwidth

Manchester-Coded FSK Data Rate and Frequency Deviation

Measured Frequency Offset

ΔfS1.5dBFSK_measured

Calculated Frequency Offset with Equation

25 kHz

0.75 kBit ±0.75 kHz±10.7 kHz±11.44 kHz
2.4 kBit ±2.4 kHz±9.4 kHz±9.10 kHz
5 kBit ±2.4 kHz±6.8 kHz±6.95 kHz

80 kHz

2.4 kBit ±2.4 kHz±35 kHz±36.6 kHz
10 kBit ±10 kHz±27.5 kHz±25.8 kHz
20 kBit ±20 kHz±17.5 kHz±11.7 kHz
165 kHz5 kBit ±5 kHz±72.5 kHz±75.4 kHz
10 kBit ±10 kHz±70 kHz±68.3 kHz
20 kBit ±20 kHz±57.5 kHz±54.2 kHz
1 kBit ±16 kHz±60 kHz±66.5 kHz
10 kBit ±16 kHz±70 kHz±63.6 kHz

366 kHz

10 kBit ±10 kHz±170 kHz±168.8 kHz
20 kBit ±20 kHz±155 kHz±154.7 kHz
10 kBit ±38 kHz±135 kHz±143.7 kHz

The following figure shows the sensitivity loss versus frequency offset for FSK with DR = 2.4 kBit/s and fDEV = ±2.4 kHz using a 80 kHz channel filter bandwidth. It can be seen that the 1.5 dB additional loss in the link budget can be avoided using a slightly higher bandwidth as already discussed in System Design with Compensation of Initial XTAL and XTO Tolerances. In the 80 kHz bandwidth, FSK DR = 2.4 kBit/s and fDEV = ±2.4 kHz case using only ±30 kHz maximum frequency offset instead of ±35 kHz avoids the additional 1.5 dB sensitivity loss in the link budget. For the other channel filter bandwidth and data rate examples, the behavior is equivalent. This can be taken into account by lowering the maximum frequency offset by BWIF/16. Equation (53) must be used to incorporate this into the system design. The ripple in the sensitivity in the following figure is caused by ±0.5 dB measurement uncertainty and is not a property of the ATA8510/15.

Figure 4-1. Measured Sensitivity Loss Versus Frequency Offset (BW = 80 kHz, FSK, DR = 2.4 kBit/s, fDEV = ±2.4 kHz)

The following figure shows the sensitivity loss versus frequency offset for DR = 10 kBit/s and fDEV = ±10 kHz using a 165 kHz channel filter bandwidth. The ripple in the sensitivity in the following figure is caused by ±0.5 bdB measurement uncertainty and is not a property of the ATA8510/15.

Figure 4-2. Measured Sensitivity Loss Versus Frequency Offset (BW = 165 kHz, FSK, DR = 10 kBit/s, fDEV = ±10 kHz)
ΔfmaxFSK⁢ =  BWIF2− DRFSK2⁢ + fDEV2⁢  −BWIF16⁢ ......(53)

The following table shows the measured and calculated maximum frequency offsets derived from equation (52) for low loss in sensitivity. Microchip recommends using these numbers for system design.

Table 4-2. Measured Frequency Offset for Low Sensitivity Loss Using an FSK System

Channel Filter Bandwidth

Manchester Coded FSK Data Rate and Frequency DeviationRecommended maximum Frequency Offset for Low Loss Based on Measurement

Calculated Frequency Offset with Equation

25 kHz0.75 kBit ±0.75 kHz±9.1 kHz±9.9 kHz
2.4 kBit ±2.4 kHz±7.8 kHz±7.5 kHz
5 kBit ±2.4 kHz±5.2 kHz±5.4 kHz
80 kHz2.4 kBit ±2.4 kHz±30 kHz±31.6 kHz
10 kBit ±10 kHz±22.5 kHz±20.8 kHz
20 kBit ±20 kHz±12.5 kHz±6.7 kHz
165 kHz5 kBit ±5 kHz±62.2 kHz±65.1 kHz
10 kBit ±10 kHz±59.7 kHz±58 kHz
20 kBit 20 kHz±47.2 kHz±43.9 kHz
1 kBit 16 kHz±49.7 kHz±56.2 kHz
10 kBit ±16 kHz±59.7 kHz±53.3 kHz
366 kHz10 kBit ±10 kHz±147 kHz±145.9 kHz
20 kBit ±20 kHz±132 kHz±131.8 kHz
10 kBit ±38 kHz±112 kHz±120.8 kHz

For ASK transmission, a frequency transient during the switching of the power amplifier has to be taken into account. At POUT= +14 dBm (PTX = 25.1 mW) and fRF = 433.92 MHz, a worst case frequency deviation of ΔfASK_max = 58 kHz with a decay time of ΔTASK = 21 µs using SUPCR.AVDIC = 0 must be considered. For FEPAC > 41, SUPCR.AVDIC is, therefore, set to ‘1’ by the configuration tool.

Using SUPCR.AVDIC = 1 at +10 dBm (PTX = 10 mW) results in ΔfASK_max = 11.7 kHz (equation (54)) in ΔTASK = 10.5µs (equation (54)). Using ASK with DR = 10 kBit/s Manchester-coded an additional frequency error of ΔfASK = ±7.25 kHz is calculated. This value is added to the ±39.05 kHz or ±81.57 kHz frequency error originated from the XTO and crystal consideration (System Design without Compensation of Initial XTAL and XTO Tolerances). The configuration tool sets SUPCR.AVDIC = 1 for a power higher than POUT = +8 dBm. If needed, this bit can be set manually to ‘1’ to get lower values of ΔfASK_max and ΔTASK for applications below POUT = +8 dBm.

For higher RF frequencies (868 MHz/915 MHz) combined with high output power of POUT = +14 dBm and high data rates, this effect can be significant. For ASK applications using Low-Band RF signals, data rates below 5 kBit/s and an output power below POUT = +10 dBm, this effect is less than ±5 kHz.
ΔfASK_⁢max⁡⁢ = 58kHz⁢  × (fRF433.92MHz)  ×PTX25.1mW⁢ ×1AVDIC⁢  + 1......(54)
ΔTFSK⁢ = 21μs⁢ ×  1AVDIC⁢   +  1......(55)
ΔfASK⁢ = ±ΔfASK_⁢max⁡⁢ ×  e1ΔTASK⁢ ×  DR⁢   ×   20......(56)
The following table shows the measured frequency offset values for 1.5 dB sensitivity loss compared with values calculated with equation (57). The calculated maximum frequency offsets are, in most cases, lower than the measured ones. Therefore, the calculated maximum frequency offsets can be used for system design using ASK.
ΔfS1.5dBASK⁢  =  BWIF2⁢ − DRASK......(57)
Table 4-3. Frequency Offset for 1.5 dB Sensitivity Loss Using an ASK System
Channel Filter Bandwidth

Manchester Coded ASK Data Rate

Measured Frequency Offset

ΔfS1.5dBASK_measured

Calculated Frequency Offset with Equation (56)

25 kHz2.4 kBit/s±11.2 kHz±10.1 kHz
5 kBit/s(1)±11.2 kHz(1)±7.5 kHz
80 kHz2.4 kBit/s±37.5 kHz±37.6 kHz
10 kBit/s±36 kHz±30 kHz
20 kBit/s(1)±36 kHz(1)±20 kHz
165 kHz2.4 kBit/s±77.5 kHz±80 kHz
20 kBit/s±66 kHz±62.5 kHz
366 kHz2.4 kBit/s±180 kHz±180.6 kHz
20 kBit/s±170 kHz±163 kHz
Note: In the case of high ASK data rates compared with the bandwidth, the sensitivity versus frequency offset curve is not as flat as in other cases. For these data rates, the frequency offset for 3 dB loss of sensitivity is given in Table 4-3 and Table 4-4.

The following figure shows the sensitivity versus frequency offset for ASK with DR = 2.4 kBit/s using 165 kHz channel filter bandwidth. The 1.5 dB additional loss in the link budget can also be avoided using the BWIF/16 lower frequency offset, as in the FSK case; therefore, equation (58) must be used for system design.

Figure 4-3. Measured Sensitivity Loss Versus Frequency Offset (BW = 165 kHz, ASK, DR = 2.4 kBit/s)
Δfmax⁢ ASK⁢  =  BWIF2⁢ − DRASK⁢ −BWIF2......(58)
Figure 4-4. Measured Sensitivity Loss Versus Frequency Offset (BW = 80 kHz, ASK, DR = 20 kBit/s)

The preceding figure shows the measured and calculated maximum frequency offset derived from equation (57) for low loss in ASK sensitivity. It is advisable to use this for system design.

Table 4-4. Max Frequency Offset for Low Sensitivity Loss Using ASK
Channel Filter BandwidthManchester Data RateRecommended Maximum Frequency Offset for Low Loss Based on MeasurementCalculated Frequency Offset with Equation
25 kHz 2.4 kBit/s±9.6 kHz±8.5 kHz
5 kBit/s(1)±9.6 kHz(1)±5.9 kHz
80 kHz 2.4 kBit/s±32.5 kHz±32.5 kHz
10 kBit/s±31 kHz±25 kHz
20 kBit/s(1)±31 kHz(1)±15 kHz
165 kHz 2.4 kBit/s±67 kHz±69.5 kHz
20 kBit/s±55.5 kHz±52.0 kHz
366 kHz 2.4 kBit/s±157 kHz±158 kHz
20 kBit/s±147 kHz±140 kHz
Note: See the description in Table 4-3.