3.4 LEDs
The functions of the six LEDs are as follows (see Figure 2-1):
- LED1 – Connected to the P0_2 pin (pin 12) of the BM71 module, which provides the status of the module
- LED2, LED3, LED4 and LED5 – Configurable test LEDs, which are low-enabled and external wire connection to the test GPIOs
- LED6 – Indicates the USB connection. This LED turns ON when the user connects the USB 5V input