2 Temporal Separation Measurement
The temporal separation is measured in the FPGA fabric logic that runs at
a 125 MHz clock. When an awvalid rising edge is detected on either one of
the FIC interfaces, a 64-bit counter is started. This counter keeps counting until the
awvalid pulse is detected on the other FIC. This counter value is read
by E51 through the APB interface, which is the actual temporal separation. The counter
values are reset back to 0 again until the next awvalid pulse arrives on
either one of the FIC interfaces. The following timing diagram shows the temporal
difference between two awvalid signals in an ideal scenario. The temporal
separation may vary based on the application.