6.3 Running the Build Script
Navigate to the microchip-tf-psa-crypto repository and run the build script with the small/medium/large/full configuration file, as needed. The example below shows a small configuration selection. This will generate the library output package pic32cmsg-psa-crypto-build in scripts/microchip.
cd microchip-tf-psa-crypto python scripts/microchip/build_library.py build --config configs/microchip/crypto-config-small.h

Available configuration files for standard profiles:
crypto-config-small.hcrypto-config-medium.hcrypto-config-large.hcrypto-config-full.h
For custom profiles, provide the path to the custom configuration header:
crypto-config-custom.h. Use the configuration files to update the
config macros as needed for the project.
Use the following command to clean/remove the build output directory:
pic32cmsg-psa-crypto-build.
# Clean build artifacts
python scripts/microchip/build_library.py clean

Use the following command only if the custom toolchain file needs to be provided. This can be avoided in a usual library build scenario where custom tools are not needed. Check scripts\microchip\toolchain for the default toolchain configuration.
# Custom toolchain path if needed
python scripts/microchip/build_library.py build
--config configs/microchip/crypto-config-small.h
--toolchain scripts/microchip/toolchain/xc32_pic32cmsg_toolchain.cmake